AXIS#.MOTOR.VRATED
Description
This parameter configures the drive for the rated velocity of the induction motor as indicated on the nameplate. AXIS#.MOTOR.VRATED is used to calculate the constant volts per Hertz characteristics of the drive and motor.
-
-
This parameter is required to be configured for AXIS#.MOTOR.TYPE = 2.
Context
For more information see Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Rotary: RPM See Velocity Units for details. |
|
Range |
Depends on units. See Velocity Range for details. |
|
Default Value |
1200 RPM Depends on units. See Velocity Units for details. |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.MOTOR.VRATED | 0x500B | 0xB | DINT | - | Velocity | RW | False |
| AXIS2.MOTOR.VRATED | 0x510B | 0xB | DINT | - | Velocity | RW | False |